Imported Waveform

The N7625B Signal Studio for LTE/LTE-Advanced TDD software enables you to load Imported Waveforms from the following waveform types that you can use to evaluate Multi-Standard Radio (MSR) effects on 3GPP LTE signals:

In the figure below, an Imported Waveform is selected for configuration. Refer to Generating an MSR Waveform.

Carrier n -- Imported Waveform

1. General

2. Baseband

Generating an MSR Waveform

Output Power Calculation (Downlink)

Power Settings (Downlink)

Overcoming Test Challenges of MSR Base Station Components and Transmitters